| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
|---|---|---|---|
| 5259h/0 | FAULT130.ACTION | M_01-04-16-000 | |
| 525Ah/0 | FAULT131.ACTION | ||
| 525Bh/0 | FAULT132.ACTION | ||
| 525Ch/0 | FAULT134.ACTION | ||
|
5267h/0 |
FAULT451.ACTION | ||
| 525Dh/0 | FAULT702.ACTION | ||
Description
This Parameter determines the action the drive should take when Fault 130, 131, 132, 134, 139, 451, or 702 occurs.
| Parameter Value | DriveControl device for regulating the speed, torque and position of a motor Action |
|---|---|
| 0 | DisableRemoval of the ENABLE signal. Disables power stage. Ampllifier |
| 1 | Ignore (fault will not be reported) |
|
Copyright © 2015 Kollmorgen™ |
|