|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current (DRV.IPEAK) |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3421h/0 |
M_01-00-00-000 |
Description
IL.FOLDFTHRESHU is the fault level of the current foldback algorithm. The value of IL.FOLDFTHRESH is the minimum of DRV.IPEAK , MOTOR.IPEAK , and IL.FOLDFTHRESHU.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|