MOTOR.BRAKERLS

General Information

Type

Command

Description

Allows a user to release or apply the motor brake.

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3450h/0

M_01-07-04-000

Description

This command allows a user to release or apply the motor brake.

0 = DriveControl device for regulating the speed, torque and position of a motor controls the brake.

1 = Brake is released.

2 = Brake is applied.

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™