MOTOR.LDLL

General Information

Type

NV Parameter

Description

Motor line to line direct axis inductance.

Units

mH

Range

1 to 2^31

Default Value

17.000

Data Type

Float

Start Version

M_01-11-00-000

Description

This parameter is the motor line to line direct axis inductance. It is supported for the IPM motor type (MOTOR.TYPE = 6).

Related Topics

Motor | MOTOR.LQLL | IL.KPDRATIO

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™