MOTOR.LISAT

General Information

Type

NV Parameter

Description

Motor quadrature axis inductance saturation characteristic.

Units

Arms

Range

0.2A to 2*DRV.IPEAK

Default Value

1000

Data Type

Float

Start Version

M_01-11-00-000

 

Description

This parameter is the quadrature axis inductance (Lqll) saturation characteristic as a function of quadrature current (Iq). It is used for q-axis current loop gain scheduling to maintain bandwidthIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz and stability during q-axis inductance saturation. This value can also be used for q-axis flux estimation during field weakening, especially for IPM motors (MOTOR.TYPE = 6).

Related Topics

Motor | MOTOR.LQLL

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™