MOTOR.VOLTRATED

General Information

Type

NV Parameter

Description

Sets the motor rated voltage.

Units

V

Range

50 to 1,000 V

Default Value

230 V

Data Type

U16

See Also

MOTOR.VRATED, MOTOR.VOLTMIN

Start Version

M_01-03-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3457h/2

M_01-03-00-000

Description

This parameter configures the drive for the induction motor's rated voltage as indicated on the nameplate.

MOTOR.VOLTRATED is used to calculate the constant Volts per Hertz characteristics of the drive and motor.

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™