SWLS.EN

General Information

Type

NV Parameter

Description

Enables and disables software travel limit switches.

Units

N/A

Range

0 to 3

Default Value

0

Data Type

U8

See Also

DRV.MOTIONSTAT

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

517Eh/0

M_01-00-00-000

Description

This parameter enables the software travel limit switches. The software limit switches are only active if the axis is homed.

Value Description
0 Disables both limit switches.
1 Enables limit switch 0.
2

Enables limit switch 1.

3 Enables limit switch 0 and limit switch 1.

If SWLS.EN = 3, then whichever limit switch is set to a greater value will be used as the upper limit switch. For all other values of SWLS.EN, use SWLS.LIMIT0 for the lower limit switch, and SWLS.LIMIT1 for the upper limit switch.

Example

Bit 0 = 0: DisableRemoval of the ENABLE signal. Disables power stage. SWLS.LIMIT0

Bit 0 = 1: EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. SWLS.LIMIT0

Bit 1 = 0: Disable SWLS.LIMIT1

Bit 1 = 1: Enable SWLS.LIMIT1

Related Topics

Limits

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™