VBUS.UVFTHRESH

General Information

Type

R/W Parameter

Description

Sets the under voltage fault level.

Units

VDC

Range

90 to 420 VDC

Default Value

90 VDC

Data Type

Integer

See Also

VBUS.OVFTHRESH

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

361Dh/0

M_01-00-00-000

Description

VBUS.UVFTHRESH sets the undervoltage fault level of the DC bus.

The default value is read from the EEPROM, but can by modified by the user and stored on the NV RAM. This value varies according to drive type.

Related Topics

Regeneration

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™