WS.DISTMAX

General Information

Type

R/W Parameter

Description

Sets maximum movement allowed for wake and shake.

Units

deg (position units)

Range

0 to 90 deg

Default Value

15 deg

Data Type

S64

See Also

N/A

Start Version

M_01-01-00-101, M_01-02-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3494h/2

M_01-00-00-000

Description

This parameter sets the maximum movement that is allowed for finding commutation. If this value is too small, FF475 , "Wake and Shake. Too much movement", may occur before wake and shake is finished. The bigger this value, the more movement is allowed for wake and shake. This value is application dependent.

Related Topics

Wake and Shake Overview

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™