ApplyRecipeColumnPLCopen motion icon

FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Apply the values of a column from a recipe file

Inputs

FILE : STRING    Path name of the recipe file (.RCP or .CSV) - must be a constant value!
COL : DINT      
Index of the column in the recipe (0 based)

 

Outputs

OK : BOOL        TRUE if OK - FALSE if parameters are invalid

Remarks

ST Language

OK := ApplyRecipeColumn ('MyFile.rcp', COL);

FBD Language

FFLD Language

(* The function is executed only if ApplyRecipe is TRUE *)

IL Language

Op1: LD"Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them               
'MyFile.rcp'
ApplyRecipeColumn COL
ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal                OK

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™