FunctionClearCtrlErrorsPLCopen motion iconPipe Network motion icon

Clears the active errors and alarms on the controller. Only clearable errors will be cleared. See PDMM and PCMM Errors and Alarms for a list of errors and alarms that may be generated.

Arguments

Input

EN Data Type EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. the function

Output

Q Data Type BOOL

Examples

FBD

FFLD

ST

//Attempt to clear active controller level errors and alarms(such as E33)
IF ClearControllerErrors THEN
ClearCtrlErrors();
END_IF;

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™