FLIPFLOPPLCopen motion icon

Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. - Flipflop bistable.

Inputs

IN  : BOOL Swap command (on rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge)
RST : BOOL ResetNew start of the microprocessor to FALSE

Outputs

Q   : BOOL Output

Remarks

The output is systematically reset to FALSE if RST is TRUE.
The output changes on each rising edge of the IN input, if RST is FALSE.

ST Language

(* MyFlipFlop is declared as an instance of FLIPFLOP function block *)
MyFlipFlop (IN, RST);
Q := MyFlipFlop.Q;

FBD Language

FFLD Language

IL Language

(* MyFlipFlop is declared as an instance of FLIPFLOP function block *)
Op1: CAL MyFlipFlop (IN, RST)
     FFLD 
MyFlipFlop.Q
     ST  Q1

See also

R   S   SR

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™