| IN | BOOL | The time counts when this input is TRUE |
| RST | BOOL | Timer is reset to 0 when this input is TRUE |
| PT | TIME | Programmed time |
| PTsec | UDINT | Programmed time. (TMUsec - seconds) |
Q : BOOL Timer elapsed output signal
ET : TIME Elapsed time
| Q | BOOL | Timer elapsed output signal |
| ET | TIME | Elapsed time |
| ETsec | UDINT | Elapsed time. (TMU - seconds) |
The timer counts up when the IN input is TRUE. It stops when the programmed time is elapsed. The timer is reset when the RST input is TRUE. It is not reset when IN is false.
(* MyTimer is a declared instance of TMU function block *)
MyTimer (IN, RST, PT);
Q := MyTimer.Q;
ET := MyTimer.ET;
(* MyTimer is a declared instance of TMU function block *)
Op1: CAL MyTimer (IN, RST, PT)
FFLD MyTimer.Q
ST Q
FFLD MyTimer.ET
ST ET
See also
|
Copyright © 2015 Kollmorgen™ |
|