IN : ANY Input value
Q : DINT Value converted to integer
For BOOL input data types, the output is 0 or 1. For REAL input data type, the output is the integer part of the input real. For TIME input data types, the result is the number of milliseconds. For STRING inputs, the output is the number represented by the string, or 0 if the string does not represent a valid number. In FFLD language, the conversion is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly Language, the ANY_TO_DINT function converts the current result.
Q := ANY_TO_DINT (IN);
(* The conversion is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
Op1: FFLD IN
ANY_TO_DINT
ST Q
ANY_TO_BOOL ANY_TO_SINT ANY_TO_INT ANY_TO_LINT ANY_TO_REAL ANY_TO_LREAL ANY_TO_TIME ANY_TO_STRING
|
Copyright © 2015 Kollmorgen™ |
|