To declare an array, enter the number of elements in the Dim. column of the Dictionary (see procedure here).
For a multi-dimensional array (note that arrays have at most three dimensions), enter the number of elements for each dimension separated by commas (for example 2,10,4 is a 3 dimensional array, the first dimension has 2 elements, the second dimension has 10 elements, and the third dimension has 4 elements).
All indexes are 0 based. For example, in the case of a single dimension array, the first element is always identified by ArrayName[0].
|
Copyright © 2015 Kollmorgen™ |
|