Below are the language features for controlling the execution of a program:
Below are the structured statements for controlling the execution of a program:
| IF | Conditional execution of statements. |
| WHILE | Repeat statements while a condition is TRUE. |
| REPEAT | Repeat statements until a condition is TRUE. |
| FOR | Execute iterations of statements. |
| CASE | Switch to one of various possible statements. |
| EXIT | Exit from a loop instruction. |
| WAIT | Delay program execution. |
| ON | Conditional execution. |
|
Copyright © 2015 Kollmorgen™ |
|