FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Converts a BCD (Binary Coded Decimal) value to a binary value
| IN : DINT | Integer value in BCD |
| Q : DINT | Value converted to integer, or 0 if IN is not a valid positive BCD value |
| IN | Q |
|---|---|
| -2 | 0 (invalid) |
| 0 | 0 |
| 16 (16#10) | 10 |
| 15 (16#0F) | 0 (invalid) |
In IL"Instruction list" This is a low-level language and resembles assembly, the input must be loaded in the current result before calling the function.
Q := BCD_TO_BIN (IN);
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
BCD_TO_BIN
ST Q
See also
|
Copyright © 2015 Kollmorgen™ |
|