CU : BOOL EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. counting. Counter is increased on each call when CU is TRUE
CD : BOOL Enable counting. Counter is decreased on each call when CD is TRUE
RESET : BOOL ResetNew start of the microprocessor command. Counter is reset to 0 called with RESET to TRUE
LOAD : BOOL Re-load command. Counter is set to PV when called with LOAD to TRUE
PV : DINT Programmed maximum value
QU : BOOL TRUE when counter is full, i.e. when CV = PV
QD : BOOL TRUE when counter is empty, i.e. when CV = 0
CV : DINT Current value of the counter
(* MyCounter is a declared instance of CTUD function block *)
MyCounter (CU, CD, RESET, LOAD, PV);
QU := MyCounter.QU;
QD := MyCounter.QD;
CV := MyCounter.CV;
(* MyCounter is a declared instance of CTUD function block *)
Op1: CAL MyCounter (CU, CD, RESET, LOAD, PV)
FFLD MyCounter.QU
ST QU
FFLD MyCounter.QD
ST QD
FFLD MyCounter.CV
ST CV
See also
|
Copyright © 2015 Kollmorgen™ |
|