FBD comments

Comment text area can be entered anywhere in an FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks diagram.

Press the following button in the FBD toolbar to insert a new comment area.

In this mode, the mouse is used to insert comment text areas anywhere in the diagram.

Double-click on the comments area to enter or change the attached text. When selected, comment texts can be resized.

          

Figure 4-85: FBD Comments - Inserting Graphic

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™