FBD corners

Corners are used to force the routing of connection lines, as the FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks editor imposes a default routing only between two pins or user-defined corners. All variable symbols and constant expressions are entered in FBD diagrams using small boxes.

Press the following button in the FBD toolbar to insert a corner on a line:

Insert corner: In this mode, the mouse is used to insert a user-defined corner on a line.

You can drag a new line from an output pin to an empty space. In this case, the editor automatically finishes the line with a user-defined corner, so that you can continue drawing the connection to the desired pin and force the routing while you are drawing the line.

Corners can then be selected and moved to change the routing of existing lines.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™