IN : STRING Character string
NBC : DINT Number of characters to extract
Q : STRING String containing the first NBC characters of IN.
In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.
In IL"Instruction list" This is a low-level language and resembles assembly, the first input (the string) must be loaded in the current result before calling the function. The second argument is the operand of the function.
Q := LEFT (IN, NBC);
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
See also
+ MLEN DELETE INSERT FIND REPLACE RIGHT MID
|
Copyright © 2015 Kollmorgen™ |
|