OR   ORNPLCopen motion icon

Operator - Performs a logical OR of all inputs.

Inputs

IN1 : BOOL First Boolean input
IN2 : BOOL Second Boolean input

Outputs

Q : BOOL   Boolean OR of all inputs

Truth table

IN1

IN2

Q

0

0

0

0

1

1

1

0

1

1

1

1

Remarks

In FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks language, the block can have up to 16 inputs. The block is called ">=1" in FBD language. In FFLD language, an OR operation is represented by contacts in parallel. In IL"Instruction list" This is a low-level language and resembles assembly language, the OR instruction performs a logical OR between the current result and the operand. The current result must be Boolean. The ORN instruction performs an OR between the current result and the Boolean negation of the operand.

ST Language

Q := IN1 OR IN2;
Q := IN1 OR IN2 OR IN3;

FBD Language

(* the block can have up to 16 inputs *)
Or FBD

FFLD Language

(* parallel contacts *)
Or FFLD

IL Language

Op1: FFLD  IN1
     OR  IN2
     ST  Q   (* Q is equal to: IN1 OR IN2 *)
Op2: FFLD  IN1
     ORN IN2
     ST Q    (* Q is equal to: IN1 OR (NOT IN2) *)

See also

AND   XOR   NOT

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™