IN : REAL/LREAL Real value
EXP : REAL/LREAL Exponent
Q : REAL/LREAL Result: IN at the 'EXP' power
Alternatively, in ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal language, the "**" operator can be used. In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.
In IL"Instruction list" This is a low-level language and resembles assembly, the input must be loaded in the current result before calling the function. The exponent (second input of the function) must be the operand of the function.
Q := POW (IN, EXP);
Q := IN ** EXP;
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
Op1: LD"Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
POW EXP
ST Q (* Q is: (IN ** EXP) *)
See also
|
Copyright © 2015 Kollmorgen™ |
|