Using the SFC toolbar

The vertical toolbar on the left side of the editor contains buttons for inserting items in the chart. Items are always inserted before the selected item, and the chart is automatically re-arranged when a new item is inserted.

Icon Description
Insert an initial step
Insert a step
Insert a transition
Insert a jump to a step
Insert the main (left side) corner of a divergence or convergence
Insert a divergence corner
Insert a convergence corner
Insert a macro-step
Insert the body of a macro-step

Table 4-20: SFC Toolbar - List of Icons

Use the following keyboard commands when an item is selected:

- ENTER: edit the level 2 of a step or transition
- Ctrl+ENTER: change the number of a step, transition or jump

The last button of the toolbar enables you to switch between possible displays:

Swap between possible overviews of level 2 in the level 1 chart:
- display code of actions and conditions
- display notes attached to steps and transitions

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™