ST / IL Language selection

The KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger allows you to mix ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal and IL"Instruction list" This is a low-level language and resembles assembly languages in textual program. ST is the default language. When you enter IL instructions, the program must be entered between "BEGIN_IL" and "END_IL" keywords, such as in the following example

BEGIN_IL
FFLD   var1
ST   var2
END_IL

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™