IN : ANY First input
MSK : ANY Second input
(XOR mask)
Q : ANY Exclusive OR mask between IN and MSK inputs
Arguments can be signed or unsigned integers from 8 to 32 bits.
In FFLD language, the input rung (EN) enables the operation, and the output rung keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly language, the first parameter (IN) must be loaded in the current result before calling the function. The other input is the operands of the function.
Q := XOR_MASK (IN, MSK);
(* The function is executed only if EN is TRUE *)
(* ENO is equal to EN *)
See also
|
Copyright © 2015 Kollmorgen™ |
|