BrakeThe brake output on connector X2 controls a mechanical brake that optionally may be fitted to a motor. The brake is applied and released relative to the DriveControl device for regulating the speed, torque and position of a motor Active state of the drive. You can modify the release and apply delays using the parameters shown below.
|
Button or Dialog Box |
Description |
Parameter |
|---|---|---|
|
Brake Control |
Sets whether the motor has a brake. |
|
|
Time to Release |
The time, set by the user, required to mechanically disengage the brake. After this time, motion commands are accepted. |
|
|
Time to Apply |
The time, set by the user, required to mechanically engage the brake. After this time, the drive will disable. |
|
Copyright © 2015 Kollmorgen™ |
|