|
Error Message |
Meaning |
Remedy |
Occurrence |
|---|---|---|---|
|
Error: Parameter or command was not found. |
Parameter or command string was not recognized as a known command. |
Check the entered string for accuracy. Consult the reference guide or enter DRV.LIST in the WorkBench terminal screen to find valid parameters and commands. |
General. |
|
Error: Not a trigger parameter. |
Parameter cannot be used for triggering the scope. |
Use a different parameter as a trigger value. |
Recorder parameters. |
|
Error: Parameter not recordable. |
Parameter cannot be scoped. |
Do not scope this parameter. |
Recorder parameters. |
|
Error: Wrong argument for parameter or command. |
Argument was not accepted. |
Check the entered argument for accuracy. Consult the reference guide or enter DRV.LIST in the WorkBench terminal screen to find valid parameter and command arguments. |
General. |
|
Error: No arguments allowed for parameter or command. |
Parameter or command supports no arguments. |
Enter parameter or command again with no arguments. |
Commands and read-only parameters |
|
Error: Too many arguments for parameter or command. |
Too many arguments provided for this parameter or command. |
Enter again with fewer arguments. |
All parameters and commands with no or one argument. |
|
Error: No float allowed. |
Float number was entered, but only integer numbers are allowed. |
Enter integer value instead. |
All parameters and commands with integer arguments. |
|
Error: Parameter or command is read-only. |
Argument was not accepted because the parameter or command is read-only. |
Enter again with no arguments. |
Commands and all read-only parameters. |
|
Error: Parameter is temporarily write protected. |
Argument was not accepted because the parameter is currently read-only. |
Check reference guide or KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger help to determine if the parameter is read-only, read-write, or nonvolatile. |
Some parameters that come from the Smart Feedback DeviceA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position (SFDSmart Feedback Device). |
|
Error: Argument greater than maximum value. |
Entered argument was beyond maximum value. |
Enter a value that is within the allowable range. See reference guide or KAS IDE help for ranges. |
Commands and read-write parameters. |
|
Error: Too many characters in parameter or command. |
Parameter or command string was too long. |
Shorten string and enter again. |
General. |
|
Error: Argument less than minimum value. |
Entered argument was too small. |
Enter value that is within the limits. |
Commands and read-write parameters. |
|
Error: Argument is out of data range. |
Entered argument was not withing the data range limits. |
Enter value that is within the limits. |
Commands and read-write parameters. |
|
Error: Parameter or command is password protected. |
Use of this parameter or command requires a password. |
Contact technical support to obtain password. Enter valid password. |
Password protected parameters and commands. |
|
Error: Wrong operation mode for parameter or command. |
Requested parameter or command cannot be performed in this operation mode. |
Change to valid operation mode. |
|
|
Error: DriveControl device for regulating the speed, torque and position of a motor enabled. DisableRemoval of the ENABLE signal. Disables power stage. drive and continue. |
Action can only be performed if drive is disabled. |
Disable drive and repeat action. |
|
|
Error: Drive disabled. EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. drive and continue. |
Action can only be performed if drive is enabled. |
Enable drive and repeat action. |
|
|
Error: Data value is invalid. |
Entered data was not valid. |
Provide valid data. |
|
|
Error: Argument must be an even number. |
Argument is not an even number. |
Enter a value divisible by two without remainder. |
|
| Error: Argument must be an odd number. | Argument must be an odd number. | Enter a value not divisible by two with remainder. | |
|
Error: Axis is not homed. |
Axis is not homed. |
Home axis and repeat action. |
|
|
Error: All recorder channels empty. |
No data is specified to record. |
Specify the data to be recorded and start again. |
Recorder commands. |
|
Error: Process already active. |
Required action is already running. |
Wait until action is finished and start again if needed. |
|
|
Error: Motor is currently in motion. |
Action can only be performed if motor is not moving. |
Stop motion and repeat action. |
Motion tasks, service motion, and others. |
|
Error: EEPROM is bad or does not exist. |
EEPROM is damaged. |
Restart drive. If fault persists, replace the drive and consult technical support. |
|
|
Error: Unknown board. |
|
|
|
|
Error: Fault exists.Correct fault condition and then clear faults. |
A fault is present in the system. |
Clear the fault, disable the drive, and then enable the drive again. |
|
|
Error: Cannot clear faults. Issue software or hardware disable first. |
|
Clear hardware or software enable and repeat action. |
|
|
Error: EEPROM is busy. |
|
|
|
|
Error: Invalid motor/feedback poles ratio. |
|
|
|
|
Error: Unknown Fault. |
Situation should not happen. |
Clear fault. If fault recurs, consult technical support. |
Unknown. |
|
Error: Invalid motor/feedback poles ratio. |
|
|
|
|
Error: Invalid motion task parameter. |
|
|
|
|
Error: Invalid motion task number. |
|
|
|
|
Error: Invalid motion task velocity. |
|
|
|
|
Error: Invalid motion task acceleration or deceleration. |
|
|
|
|
Error: Invalid motion task customer profile table number. |
|
|
|
|
Error: Invalid motion task following number. |
|
|
|
|
Error: FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. not available for the active command source. |
|
|
|
|
|
|
|
|
|
Error: Invalid sine-sweep Bode plot mode. |
|
|
|
|
Error: Bode plot start frequency greater than or equal to end frequency. |
|
|
|
|
Error: Function not available while a controlled stop is in process. |
|
|
|
|
Error: Not enough memory available. |
|
|
|
|
Error: Function not available while a Bode-plot measurement is active. |
|
|
|
|
Error: Iu/Iv offset calculation not finished. |
|
|
|
|
Error: Buffer overflow. |
|
|
|
|
Error: Cannot save to EEPROM while inrush relay is closed. |
|
|
|
|
Error: Test mode is off. |
|
|
|
|
Error: Cannot change digital input mode. Issue software or hardware disable first. |
|
|
|
|
Error: Internal drive procedure active: controlled stop, burn-in, phase find, or zero. |
|
|
|
|
Error: General motion fault. |
|
|
|
|
Copyright © 2015 Kollmorgen™ |
|