Based on the File Access over EtherCAT (FoE) protocol, the AKD drive Firmware can be downloaded as follows:
AKD-N-xxEC-********.i00 supports multiple AKD-N models. 

Give careful attention to any warning dialog that appears at this point. These warnings usually include important information about preventing damage to the drives.
This procedure is not possible when applications are running and when the drive is in Online Configuration Mode.
During the firmware download, the AKD Firmware Update window displays a progress bar and the following messages are displayed:
While the firmware is downloading to your drive, do not remove the 24V logic power. If you remove the 24V logic power during a firmware download, a severe drive crash can occur. If a crash occurs, the drive will restart in a special mode and prompt you to reload the firmware.
An AKD drive executing the resident firmware is detected as a different device than an AKD drive executing the operational firmware. Be sure to re-scan the network and compile it if a drive's executed firmware has changed since the last scan.
Power cycling is recommended after completing the update for all drives.
|
Copyright © 2015 Kollmorgen™ |
|