FunctionMLAxisAbsPipe Network motion icon

Description

Performs a move to an absolute position. Returns TRUE if the function succeeded.

Arguments

Input

ID

Description

ID name of the Axis Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

Position

Description

Sets the value of the absolute destination position.

When the Modulo is turned on, see more explanations below.

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Position with Modulo On

When the Modulo is turned on, the Axis Block moves to the targeted position during the corresponding period, calculated as follows:

The Axis Block works similarly for negative positions: if the Position input is less than zero, then the Axis Block moves during one of the previous period (negative position rollover).

Forcing the direction of rotation

In some applications, the direction of rotation for the axis is forced in one direction only. As a consequence, the motor movement goes to the next or previous modulo in the following situations:

Examples

Start Position End Position Direction of rotation Cross Modulo Position Input to MLAxisAbs (1) RelativeDistance Moved (2)
60 200 clockwise No 200 140 (i.e. 200 - 60 + 0)
60 30 clockwise Yes 390 330 (i.e. 30 - 60 + 360)
60 30 counter clockwise No 30 -30 (i.e. 30 - 60 - 0)
60 200 counter clockwise Yes -160 -220 (i.e. 200 - 60 - 360)

With:

(1) Position Input = End Position ( + Modulo * Direction of rotation)

 

(2) Relative Distance Moved = End Position - Start Position ( + Modulo * Direction of rotation)

Where:

Direction of rotation = 1 when clockwise and -1 when anti-clockwise

Travel Speed Update with MLAxisAbs

The travel speed of the generator can be updated using the function block MLAxisGenWriteSpd. Depending on the state of the generator, this speed is directly reflected on the current move or a future move.

Following are several examples.

  1. First MLAxisAbs
  2. Second MLAxisAbs
  3. Initial Speed
  4. New Speed

Figure 11-73: Initial speed is smaller than the new speed

  1. First MLAxisAbs
  2. Second MLAxisAbs
  3. Initial Speed
  4. New Speed

Figure 11-74: Initial speed is bigger than the new speed

  1. Acceleration
  2. Constant Velocity
  3. Deceleration

Figure 11-75: The speed update is taken into account only if the second MLAxisAbs is triggered during acceleration or constant velocity

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLAxisGenWriteSpd

MLAxisGenWriteDec

MLAxisGenWriteAcc

Example

See Usage Example of Axis Functions for additional examples.

Structured Text

 

MLAxisAbs( PipeNetwork.Axis1, 2000 ) ;

 

Ladder Diagram

MLAxisAbs: LD example

 

Function Block Diagram

MLAxisAbs: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™