FunctionMLAxisAddressPipe Network motion icon

Description

Returns the motion bus address of the axis. It is possible that two or more axes have the same address if the axis is mapped to a multi-axis drive, such as the dual-axis AKD2G drive.

Arguments

Input

ID

Description

ID name of the Axis Block

 

Data type

DINT

 

Range

 

Unit

n/a

 

Default

Output

OK

Description

Returns true when function successfully executes

 

Data type

BOOL

 

Unit

n/a

Default (.Q)

Description

Returns the motion bus address of the axis

 

Data type

DINT

 

Unit

n/a

Example

Structured Text

Axis1_Address := MLAxisAddress(PipeNetwork.AXIS1);

Ladder Diagram

Function Block Diagram

MLAxisAddress: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™