FunctionMLAxisInitPipe Network motion icon

Description

Initializes an axis object. Returns TRUE if the function succeeded

Arguments

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

 

Unit

n/a

 

Default

ModuloPosition

Description

Value of the period of a cyclic system expressed in user units. The parameter is defined to correctly manage the periodicity (modulo) of the input values

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

UserUnitPerTurn

Description

Define the unit which is equivalent to one revolution of the physical motor

 

Data type

LREAL

 

Range

 

Unit

n/a

 

Default

FeedbackUnitPerTurn

Description

 
 

Data type

DINT

 

Range

 

Unit

n/a

 

Default

Speed

Description

Sets the Axis Speed

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Acceleration

Description

Sets the Axis Acceleration value

 

Data type

LREAL

 

Range

 

Unit

User unit/sec2

 

Default

Deceleration

Description

Sets the Axis Deceleration value

 

Data type

LREAL

 

Range

 

Unit

User unit/sec2

 

Default

InitialPosition

Description

Initial position value expressed in user logical units. Used only at the pipe activation to initialize the position starting point

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Modulo

Description

Define the mode which can be Modulo (True) or not (False)

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Example

Structured Text

MLAxisInit( PipeNetwork.Axis1, 360.0, 360.0, SHL(1,20), 500.0, 100000.0, 100000.0, 0.0, true ) ;

Ladder Diagram

MLAxisInit: LD example

 

Function Block Diagram

MLAxisInit: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™