MLAxisRelA selected Axis performs a move for a specified distance relative to the current position. The DeltaPosition input is signed so that the move can be in the positive or negative direction, and the Axis moves this distance in user units. The travel speed, acceleration, deceleration, and User Units of the move are values inherited from the selected Axis. The default settings are entered when an Axis is created and initiated, and can be changed with other MLAxis commands such as MLAxisGenWriteSpd, MLAxisGenWriteAcc, and MLAxisWriteUUnits.
If you wish to know when a move has completed, we recommend using MLAxisGenIsRdy. The output of MLAxisRel can occur before moves have finished.
|
ID |
Description |
ID Name of the Axis block |
|
Data type |
DINT |
|
|
Range |
— |
|
|
Unit |
n/a |
|
|
Default |
— |
|
|
DeltaPosition |
Description |
Sets the Axis Delta Position, or the relative distance to be moved |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
||
|
Default |
— |
|
Default (.Q) |
Description |
Returns true when function successfully executes. This occurs immediately after the function is called; the function does not wait for the motion profile to be completed. See more details here |
|
Data type |
BOOL |
|
|
Unit |
n/a |
See Usage Example of Axis Functions for additional examples.
|
MLAxisRel(PipeNetwork.Axis1, 2500 ) ;
|
You must use a pulse contact to start the FB
|
Copyright © 2015 Kollmorgen™ |
|