FunctionMLAxisWritePosPipe Network motion icon

Description

Used to set a position offset at the Axis when the Pipe Network:

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

 

Unit

n/a

 

Default

Position

Description

Position offset.

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Previous Function Name

MLAxisSetZero

Example

Structured Text

 

MLAxisWritePos( PipeNetwork.Axis1, 0) ;

 

Ladder Diagram

MLAxisWritePos: LD example

Function Block Diagram

MLAxisWritePos: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™