Function BlockMC_ReadBoolParPLCopen motion icon

Description

The MC_ReadBoolPar function block returns the value of the specified Boolean axis parameter.

MC_ReadBoolPar

Figure 11-124: MC_ReadBoolPar

Arguments

For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules

Input

EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive.

Description

Requests to read the Boolean axis parameter

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

Axis

Description

Name of a declared instance of the AXIS_REF library function. For more details, About Axis Name and Number)

 

Data type

AXIS_REF

 

Range

[1,256]

 

Unit

n/a

 

Default

ParameterNumber

Description

Parameter number, see table in Axis Parameters

 

Data type

INT

 

Range

 

Unit

n/a

 

Default

Output

Valid

Description

Indicates the Value output is valid

 

Data type

BOOL

Busy

Description

Indicates this function block is executing

 

Data type

BOOL

Error

Description

Indicates an invalid input

 

Data type

BOOL

ErrorID

Description

Indicates the error if Error output is set to TRUE

See table in PLCopen Function Block ErrorID Output

 

Data type

INT

Value

Description

State of the Boolean parameter

 

Data type

BOOL

Example

Structured Text

(* MC_ReadBoolPar ST example *)
Inst_MC_ReadBoolPar( EnableRead, Axis1, MC_AXIS_PARAM_IN_POSITION );
Axis1InPosition := Inst_MC_ReadBoolPar.Value;

Ladder Diagram

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™