FunctionMC_ResetErrorPLCopen motion icon

Description

The function MC_ResetError resets the errors of a specified axis.

This function performs in sequence the following tasks:

See also transition 15 in the status machine of the CANopen protocol.

MC_ResetError

Figure 11-118: MC_ResetError

Arguments

For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules

Input

En

Description

Requests to reset the axis errors

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

Axis

Description

Name of a declared instance of the AXIS_REF library function (for more details, About Axis Name and Number)

 

Data type

AXIS_REF

 

Range

[1,256]

 

Unit

n/a

 

Default

 

Output

OK

Description

Indicates the function has completed successfully

See more details here

 

Data type

BOOL

Example

Structured Text

//reset the axis and drive errors for Axis 1
MC_ResetError( Axis1 );

Ladder Diagram

MC_ResetError: LD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™