MLPmpAbs
| BlockID | Description | ID Name of the PMP function block in the Pipe Network |
| Data type | DINT | |
| Range | [-2147483648, 2147483648] | |
| Unit | n/a | |
| Default | — | |
| Position | Description | Absolute Position of motor/load to be at after this FB is complete |
| Data type | LREAL | |
| Range | — | |
| Unit | User unit | |
| Default | — |
|
Default (.Q) |
Description | Returns True if the function block is successfully executing See more details here |
| Data type | BOOL | |
| Unit | n/a |
|
MLPmpAbs( PipeNetwork.PmpMaster, 1000.0 ) ;
|
|
Copyright © 2015 Kollmorgen™ |
|