Open topic with navigation
State Machine
Figure 6-63: EtherCAT State Machine
Where the transitions are:
- from Init to Pre-Operational (Pre-Op): Master configures the Sync Manager channels for Mailbox communication
- from Pre-Op to Safe-Operational (Safe-Op): Master configures parameter using the Mailbox
- from Safe-Op to Operational (Op): Master sends valid Outputs
The different states are:
- Init
No communication on the Application Layer
Master has access to the DL-Information registers
- Pre-Operational (Pre-Op)
Mailbox communication on the Application Layer
No Process Data communication
- Safe-Operational (Safe-Op)
Mailbox communication on the Application Layer
Process Data communication. Only Inputs are evaluated (Outputs in Safe state)
- Operational (Op)
Inputs and Outputs are valid
- Bootstrap
Recommended if firmware updates are necessary
No Process Data communication
Communication via Mailbox on Application Layer
Only FoE protocol available
See Also
|
|
Copyright © 2015 Kollmorgen™
|
|
|
Open topic with navigation