With the above-mentioned basic building blocks, a program can be seen as a network of functions and function blocks. Each of them being written in any of the defined programming languages.
The list of programs is completed with "Sub-programs". Sub-programs are written in FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks, FFLD, ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal or IL"Instruction list" This is a low-level language and resembles assembly languages, and can be called by the programs of the application. Input and output parameters plus local variables of a sub-program are declared in the variable editor as local variables of the sub-program.
Unlike UDFB, local variables of a sub-program are not instantiated. This means that the sub-program always works on the same set of local variables. Local variables of a sub-program keep their value among various calls. The code of a sub-program is not duplicated when called several times by parent programs.
A sub-program cannot have more than 32 input parameters or 32 output parameters.
A good programming practice is to break up your programs into smaller modules.
See also Application Software Structure - Definitions.
An application is a list of programs. Programs are executed sequentially within the target cycle, according to the following model:
Begin cycle | exchange I/Os | execute first program | ... | execute last program | wait for cycle time to be elapsed End Cycle
Programs are executed according to the order defined by the user. All SFC"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions programs must be grouped (it is not possible to insert a program in FBD, FFLD, ST or IL between two SFC programs). The number of programs in an application is limited to 32767. Each program is entered using a language chosen when the program is created. Possible languages are Sequential Function Chart (SFC), Function Block Diagram (FBD), Free Form Ladder Diagram (FFLD), Structured Text (ST) or Instruction List (IL).
Programs must have unique names. The name cannot be a reserved keyword of the programming languages and cannot have the same name as a standard or "C" FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. or function block. A program must not have the same name as a declared variable. The name of a program must begin by a letter or an underscore ("_") mark, followed by letters, digits or underscore marks. It is not allowed to put two consecutive underscores within a name. Naming is case-insensitive. Two names with different cases are considered as the same.
You can define a hierarchy of SFC programs, entered as a tree in the list of programs. A child program is controlled within action blocks of the parent SFC program.
Even if you do not want to split your FFLD program, at least separate FFLD from SFC. Simply make a sub-program in FFLD called from the SFC step, and keep only the state machine in the SFC program. This makes everything simpler and more comfortable for editing and debugging.
When creating your application you have to consider the following important limitations.
For any program, sub-program or UDFB written in other languages:
|
Copyright © 2015 Kollmorgen™ |
|