Map Variables to HMI

For HMI"Human-machine interfaces " Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response, the variable mapping is done in two phases.

The tag operation directly takes place in the Dictionary, as follows:

  1. Open the Variable list editor available in the Dictionary toolbox
  2. In the KVB column, select the variables you want to map

    Variable Mapping to HMI

  3. Figure 5-29: Variable Mapping to KVB.

  4. Compile the application to create the Modbus mapping file.
  5. Open the KVBProject from the Project Tree. This will automatically transfer the tagged variables..

List of variables that you can export

The following types of variables can be exported to the HMI:

Examples of structures that you can export

Examples of structures that you cannot export

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™