PLC Variable Creation Wizard

This wizard allows you to automatically create a list of variables used for the mapping. The variable type is Boolean for digital I/Os and UINT for analog I/Os.

Wizard to Create PLC Variable - Parameters

Figure 5-104: Wizard to Create PLC Variable - Parameters

Field Description
From channel Defines the range of channels you want to map automatically
Scope Defines where the variables are created (if you select the Global scope, then the variables are created under the Global node in the Dictionary)
Base Name Pattern used for variable naming with the name of the object in the Project Tree, followed by a 2-letter acronym (2LA) representing the I/O type. The channel number will replace ##.

Wizard to Create PLC Variable - Mapped Channels

Figure 5-105: Wizard to Create PLC Variable - Mapped Channels

Wizard to Create PLC Variable - Variables in the Dictionary

Figure 5-106: Wizard to Create PLC Variable - Variables in the Dictionary

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™