Mapping Variables to the Control Panel

To map the variable:

  1. Select the variable in the Dictionary toolbox
  2. Move it to the control to be linked in the Control panel editor using drag-and-drop

    Map Variables to an HMI Control in the Graphical Editor
  3. Figure 10-37: Map Variables to a Control Panel Control in the Graphical Editor

The Variable symbol is automatically updated in the Properties tab.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™