This tab enables you to search for all the instances of a string of characters (search is not case sensitive) within the entire environment, and replace it if desired.
You can re-use one of the last ten entries or type a new text string.
| Call out# | Description |
|---|---|
|
The operation can be performed across:
|
|
The search string can be with 'complete word' only. When selected, only the instances that match the complete words defined in the "Find what" field are selected (for example, a search for "MyVar" returns "MyVar" but not "MyVariable"). When this option is selected, the search is case sensitive. |
|
To optimize your project, the Find Unused Variables option allows you to perform a search in the dictionary to locate variables not used 1 A variable is not used when there is no effective usage of it in your entire project.It can still be the case even when a value is assigned to a variable (e.g. MyVar := 100. * Axis1.Velocity ;).The variable MyVar becomes used when it is affected as an input argument (e.g. Velocity := MyVar ;). in any program. Double-click a variable in the list within the table widget to open it in the Dictionary. |
|
With the Replace... button, you can replace in all documents a string with another one (or re-use one of the last ten entries)![]() The replace function is limited: it is not supported in the Dictionary, Pipe Network and HMI"Human-machine interfaces " Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response. For those, you have to make the change manually. |
Once the search is done, the results appear in the table widget at the bottom of this tab. If a replace has been performed, the Text column provides more information about the replacement.
Double-click the item you want in the list in order to open it in its relevant location (it can be a PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events editor or the Dictionary).


FFLD Location details

ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal Location details

For more details, see "Find and Replace Operations".
|
Copyright © 2015 Kollmorgen™ |
|