Tools Menu

Command

Description

Oscilloscope

Show the soft oscilloscope

Compile (Ctrl + B)

Compile the whole project

User Options

Open the User Options dialog box.

Table 5-5: Tools Menu Commands

User Options

The check box found in this dialog enables/disables the “Load at startup” option in the AKD GUI"Graphical User Interface" A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices Scope “settings” tab.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™