ST Editor Keyboard Shortcuts

ST Editor (common)

Shortcut Command
Arrows Move caretThe term caret is also sometimes used in graphical user interface terminology where it means a text insertion point indicator, frequently represented by a blinking vertical bar. In this context, it may be used interchangeably with the word cursor, although the latter term is often reserved for a mouse pointer
Shift + arrows Selection
Ctrl + left/right arrow  Go to previous/next word
Shift + Ctrl + left/right arrow Select previous/next word
Ctrl+F2 Toggle Bookmark (Note that you first have to select the Network header)
Shift+F2 Go to Next Bookmark
Ctrl+Shift+F2 Go to Previous Bookmark

Table 5-17: List of ST Shortcuts

ST Editor (when editing)

Shortcut Command
. Select member of a structure or instance
Ctrl + Spacebar Auto completion or Open the variable selector dialog
Ctrl + Shift + Spacebar Opens a list of all the standard functions
Ctrl + J Auto completion or Open the variable selector dialog (an alternative method)

ST Editor (during debug)

Shortcut Command
* Lock variable
/ Unlock variable
Shift + double-click Force a variable
Spacebar Toggle Boolean value or bring the dialog to force, lock, unlock the variable (equivalent of Shift + double click)

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™