|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the drive operation mode (current, velocity, or position). |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
Description
DRV.OPMODE specifies the operation mode of the drive. You must also use DRV.CMDSOURCE to set the source of the command to the drive.
The operation mode values can be set as follows:
|
Mode |
Description |
|---|---|
|
0 |
Current (torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist) operation mode |
|
1 |
Velocity operation mode |
|
2 |
Position operation mode |
DRV.OPMODE can be changed while the drive is enabled or disabled. If you are using the terminal to change the operation mode, then it is recommended that you disable the drive before changing the operation mode. If you change the operation mode from the terminal while the drive is enabled, the system may experience a step change in demand.
Example
Set the source of the command to a TCP/IP channel and the desired operation mode to velocity:
-->DRV.CMDSOURCE 0
-->DRV.OPMODE 1
Related Topics
1 Current Loop
1 Velocity Loop
1 Position Loop
|
Copyright © 2015 Kollmorgen™ |
|