|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the motor peak currentThe effective value of the peak current. |
|
Units |
mA |
|
Range |
0.200 to 1,000 A |
|
Default Value |
2.000 A |
|
Data Type |
Float |
|
See Also |
IL"Instruction list" This is a low-level language and resembles assembly.LIMITP, IL.LIMITN |
|
Start Version |
M_01-00-00-000 |
Description
This parameter configures the drive for the motor's peak, instantaneous-rated current. MOTOR.IPEAK is used to limit clamp the magnitude of the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing q-component current command (IL.CMD ).
This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|