MOTOR.PHASE

General Information

Type

NV Parameter

Description

Sets the motor phase.

Units

Electrical degrees

Range

0 to 360°

Default Value

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Description

This parameter sets the motor phase.

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™