MOTOR.PITCH

General Information

Type

NV Parameter

Description

Sets the motor pitch.

Units

mm

Range

1 to 1000mm

Default Value

32mm

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Description

This parameter defines the pole-to-pair pitch for the linear motor in millimeters.

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™