MOTOR.R

General Information

Type

NV Parameter

Description

Sets the stator winding resistance phase-phase in ohms.

Units

Range

0.001 to 650 Ω

Default Value

10 Ω

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Description

MOTOR.R sets the stator winding resistance phase-to-phase in ohms.

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™